Hello,
I can’t start a .urp program via the dashboard server on an UR20.
The dashboard server returns “Failed to execute: play"
- robot is in remote mode
- all other dashboard server commands e.g. ‘stop’ do work.
- .urp program is loaded. I also reloaded it via the ‘load <program.urp>’ command.
- i have a hardware start button. That works.
Is there something I missed? How can I make it work?
I’m using URSim for a UR5 and am getting the same issues. I’m even putting delays between the commands to make sure it’s not because the program hasn’t finished loading, but it always fails. I also tried stopping any programs that may be executing to blocking the one I want to run, but to no avail thus far.
Yes! I set mode to automatic (aka remote as far as I can tell from the documentation). I suspect the issue actually comes from the Automove at the start which requires me to use the teach pendant in the sim to move the robot to it’s starting position. I tried setting a Home Point and using a BeforeStart sequence, but that still didn’t resolve the issue
automatic is not remote mode. you need to enable remote mode from the settings (not the installation)
try starting with a relative move. either a direction node or teach a relative waypoint. it will allow you to bypass the automove input.