Hello, I would like to program an application in the installation tab where the user is guided through three steps to calibrate a plane, similar to the existing teach-in function for planes. Is it possible to develop a teach function by myself and if yes how?
Thank you in advance.
You can enable freedrive and disable it again from within a program through script commands, and then save the position to a variable. So if you can make do with teaching through freedrive, then it could work like this.
But your issue is probably going to be adjusting the plane with the positions. As far as I know, it’s not possible to adjust planes/features from a running program. I have tried to do this myself before. ![]()
Maybe somebody else has more insight. Or any good ideas.