Dear UR+ maintainers,
As a UR+ developer, I’d like to have the ability to create linked (fixed) waypoints using the SDK as a user would do manually.
This would help with the automatic generation of program templates that need to move to the same user-defined waypoint more than once during the program execution, giving the user the possibility of using fixed-waypoint features such as Move here, Set position, etc.
Some extra considerations:
- One possibility that would be backwards compatible could be adding a
booleanargument tocreateWaypointNodemethod inProgramNodeFactory. If the argument istrue, the method would link the created waypoint instead of changing the suggested name if a waypoint already exists with the same name. - The original post with some more details and a workaround can be found here. As of API 1.7, creating a combination of fixed and variable waypoints could be a workaround for simple use-cases, but having the ability to create linked waypoints would be more convenient and consistent to the end-user.
Finally, please let me know if you need more details or clarifications about the feature request.
Thanks in advance!