Hello, I am new here, currently working with an UR5.
I need to configurate or implement a gui for the teach pendant wich the user may input some variables and run a define script.
Just from what I can tell through these photos you 100% can accomplish it. You’ll most likely want to work with the installation screen of the UR.
Each operation will have a corresponding function, quantity and the toggle can both be functions for each operation. I would go with the function approach over lets say a global variable because it’s unchangeable by the operator. You’ll want to look at the function model api to accomplish this.
Then in your program tree you’ll just have to set it up to work along side all these functions.
Do you want to implement a custom HMI in the “Run program” menu to make it available to the operators or do you want to make a custom functionality available to the programmer in the “Program robot”?
At the moment with the UR SDK you can only add new functionality in the “Program robot” menu, you cannot make a custom GUI for the operator.
@anon90783502 Is this supported on the latest SDK yet? I am looking at doing a similar GUI (out of Run Program) to enable operators to adjust Robot positions and change recipes.
Is this possible yet?
I have looked through a couple of posts on here but haven’t really gotten a clear picture yet. Some people seem to have been able to hack something together but nothing concrete, would be glad for any pointers
Something like this will be available once UR launches PolyscopeX later on this year. It was demonstrated at a trade show a few months ago and will offer functionality very similar to that requested in this post!