Hi all,
I am trying to set up a connection between CODESYS and URSIM 5.6, using the network Ethernet/IP adapter.
I have a VM in Oracle running URSIM 5.6, I have started the Ethernet IP Adapter and get to the point in which I have the yellow light, meaning the adapter is running but not connected.
In the network settings of the Virtual Machine I configured the Host Only Adapter, from inside the VM if I run the command ifconfig my IP address is 192.168.56.101 .
Outside the VM, in my Windows OS, I installed CODESYS, created a Standard Project and using the .edf file provided by UR I installed the Universal Robots device, obtaining the following program structure 
From Windows the IP address of my HostOnly Network adapter is 192.168.56.102.
For this reason In the ethernet device I set that IP address as shown in the picture below:
As it concern the Universal_Robot device I set the IP address as 192.168.56.101 (the one seen inside my VM)
When I run my program The Ethernet device and the Ethernet IP Scanner seems to work fine but the Universal_robots device fails (as you can see in the first picture ), the log is the following:
Has everyone ever tried to use Codesys with URSIM and suceeded?
In a normal situation I would have tried to make it work with a real robot, not URSIM, to understand if the problem relies in the use of the VM or in my configuration in CODESYS but unfortunately I am not able to access the robots in the office any time soon.
Thanks for the help,
Best regards,
Castelli Pietro