Hello,
i have the following setup: Two UR10e Robots in the same safety area with a fence with 2 doors around. Now i want 2 Emergancy Stop buttons and 3 Safeguard reset Buttons.
I saw that u can connect the two Robots so when one gets a emergency Stop, both will stop. But the Problem is in my setup that sometimes only one Robot is powered on so thats not a solution.
My idea is to bridge the +24V from the emergancy stop clamp from UR10e Nr. 1 with the +24V from UR10e Nr. 2 and bridge again on the 11 contact from the emergancy stop. The same with the second Channel.
Than with the 12 contact from the Emergancy stop → bridge to the emergancy input from UR10e Nr.1 and Bridge again with UR10e Nr. 2.
The same with the Reset buttons.
i Would bridge the 0V from UR10e Nr. 1 with UR10 Nr. 2.
The Question is, is this a working solution?
Is it ok to bridge the 24V from UR10e Nr. 1 with the 24V from UR10e Nr. 2? Or is there a technical fault so i would crash my 24V clamps :D?
Thanks for your help!!