Hello, where can I find latest version of urmagic backup program? does this script also save the robotiq wrist camera and vacuum grippers infos? Initialisation and variables files are also saved? Thanks a lot.
urmagic files have not been changed for a very long time (as far as I know). backup programs will only save programs and Installation files.
The URCap settings are stored in the Installation file, so they will be backed up, as well. Not sure what you mean by “initialisation”, but if it’s Default Program, then yes. It’s in the Installation section along with variables.
How about you do a quick test yourself to see what is saved? It’s fairly straightforward. ![]()
I will do that. My only concern is that the script might delete something at some point and in situation that i dont have enought space on the polyscope maybe thus files got corrupt.
The script will not corrupt anything. I have used it hundreds of times without issue. ![]()
A better way to backup on newer versions of Polyscope (also 3.14) is to use the Support File in the Log tab. This will backup all programs and installation files, as well as calibration files and a lot of other stuff.
Regarding your update from 3.14 to 3.15 - no data is lost when updating. It is still a good idea to backup first, of course.
Just use the Support File function.