Hi, I am looking for a method for allowing free motion in the Y direction while the robot moves the tool down in the Z axis. The aim is for the robot to insert a tool into a hole, however the alignment can sometimes be slightly out in the Y direction. To avoid damage I am trying to write code for the insertion to continue in the Z axis, but the presence of the hole wall will direct the tool into correct alignment, it will not try to resist motion in the Y direction.
Currently the tool head will moveL in Z and if it experiences too much force will abort the operation and move away.
I’d reccomend a hardware change here. Since your looking to use force on a CB3 (no force torque sensor) you should consider buying one. I can reccoment the Robotiq force torque sensor, it’s pricy but does a great job.
I do have a robotiq force torque sensor on the CB3. Currently I am telling the robot to record the force in the X and Y as it inserts, if it then aborts due to an excessive force in Z it will record the X and Y forces and using these it can almost determine which direction it needs to move to complete a successful second insertion.
I am trying to see if there is a way for it to “freedrive” in X and Y as it descends in Z, or if I will just have to code this via lots of little translations.
Without using RTDE I guess you can’t supply the built in Force template with an external force sensor data.
For a script version I guess you can look at the Z position as the end goal, trigger a slight upwards movement if the Z stops to early then mode sideways a little in a little outward spiral pattern or something every time it doesn’t reach the desired Z position.
Depending on the shape of the hole you’re trying to hit you can also detirmine if you need to move in X or Y by looking at the force in your sensor.
Magnus - As far as I remember, the Robotiq URCap for the FT300 does overwrite the Force template sensor data (or you can enable it as an option?). Or are you completely sure that isn’t the case?
I’d have to wire up one and test, it’s been a while since I’ve had to use force on a CB3 so you could be right.
I’ll see if I can get around to doing so.