After updating POLYSCOPE to 5.17.0 Network setting: Screen is locked by PROFINET/PROFISafe

POLYSCOPE version: 5.17.0
Robot: UR5e

Once updating POLYSCOPE from 5.5 to 5.17.0, the network setting is locked as: Screen is locked by PROFINET/PROFISafe.
I do not know or activate or set or use the PROFINET/PROFISafe feature at all before and after the version update.


I failed to set any of these IP configurations after inputting the admin password.

Problem solved.
It happens that the Installation-> Field bus-> PROFINET is automatically enabled after the software update.
After I deactivated the PROFINET (Remember to save and coverthe default installation after this change), the Network setting is available again.

I am not expected that the PROFINET bus is enabled, even I haven’t purchased and opened it.