Hello all. I am currently trying to communicate with a vention 7th axis rail system connected to a UR20 using Grasshopper. I was wondering if there was a way to do this and how it could be done? I am currently using the Machina plugin in grasshopper to communicate with the robot arm, but I simply want to move the rail for now as I’m aware that UR robots currently don’t support external axis systems in Machina. Thanks!
Machina is great, but its also 6 years old at this point.
You might want to check out the Robots plugin ( GitHub - visose/Robots: Create and simulate ABB, KUKA, UR, and Staubli robot programs. · GitHub )
You can then send commands to the rail using this method:
I’m running into a problem where if i have two commands (i.e. continuous move and home command for vention rail) it will not execute it at all. It will work if only one is applied but it will not even move the robot if two are connected.
Hello again, I have continued to work on this project and I realized I forgot to mention I am attempting to have both robots (rail and arm) to move at the same time. Is this possible? Don’t the commands inserted into the target creation block perform the entire command first and then moves on to the next target? I’ve been stuck on this for a while