Undocumented URScript commands

I don’t know if there are other sources to find some of the commands available which aren’t included in the URScript manual.

I can think of a handful right off -

Var1 = request_boolean_from_primary_client(“description string”)
Var1 = request_float_from_primary_client(“description string”)
Var1 = request_integer_from_primary_client(“description string”)
Var1 = request_string_from_primary_client(“description string”)

anyone else have more that might be useful?

The commands you have listed are documented in the latest versions of the URScript manual

image

well this might be usefull for everyone using ursim and testing their programs.

works ONLY with URSim:

exchange the _out with _in and you can easily force INPUTS
set_standard_digital_in(n,b)

works for all IO´s, analog IO, tool IO…

Thanks - didn’t realize there was a new version out - I was looking at the 5.15 version that I downloaded in May.