Hello, I have an issue, Im trying to power a solenoid with 2 sources. The first source is a hoist controller off amazon. I wanted a wireless remote and figured that was the cheapest way. Second source is my UR10 cobot, from what I understand is that this gives out a 24v signal but I has its own separate ground. More importantly, I do not want power being sent back to the cobot (If i just spliced the 2 inputs.). Current plan is to use a relay, but in a way that im not sure is right. I want to have power come in to the NC and the NO plugs and then, where the power normally enters, Ill attach the positive of my pneumatic solenoid. From there I will attach the switched power from my cobot to one side of the coil and the other to my cobot ground.
Will this work as a way to isolate my robot from the 24v system that controls my pneumatics? Im sure a PLC is probably the right choice but im not making money off of this so its hard for me to throw a bunch of money at it. If theres a better way, I would love to hear it. I just bought a UR10 from an auction so I could learn programing and other automation. So feel free to state the obvious.