I have set up the robot correctly in a virtual machine on my computer and am trying to send the program and installation to the physical robot via a usb stick. However, the installation is incomplete as the features are not transferring over. Is there a good method to fully transfer information from the computer to the robot.
What exactly is the error/issue? Features should be saved to the Installation, which gets saved alongside the .urp file. You should be able to just copy the urp, variables, and Installation file to your robot.
Thanks for the help, must have been a bug. I restarted everything, and it seemed to work.