mvrooij
1
Dear,
Following code:
Jp1 = [ set of 6 joint values ]
p1 = get_forward_kin(Jp1)
p2 = get_forward_kin()
def get_dif(a,b)
dv = [ b[0]-a[0],b[1]-a[1],b[2]-a[2] ] <- I get syntax error on this line. Why???
return dv
end
Then I call:
d = get_dif(p1,p2)
The result is a syntax error…
If I’m not allowd to take the difference, how should I do it then?
Thanks,
Max
mvrooij
2
A minor update:
I’ve cahnged get_dif() to:
det get_dv(a,b)
dvp = pose_sub(b,a)
dv = [ dvp[0], dvp[1], dvp[2] ]
return dv
end
Would this solve the problem?
Ok, case closed…
I’m really embarrased by this, but I forgot the ‘:’ after the line def get_dv() …whoops…
system
Closed
4
This topic was automatically closed 2 days after the last reply. New replies are no longer allowed.