- How can I select an UR-Programm from my Siemens PLC 1200 using the Profinet Interface?
- Is it possible to start an UR-Programm without using the teach pendant? (ON → select programm → reset the UR → start)
Check the other question asked a couple of days ago regarding MODBUS. It’ll be the same procedure for PROFINET. ![]()
But you can set up a dashboard connection through TCP/IP socket communication in the PLC 1200, if you want to go that way. Then you can load programs and start them with commands.
You will have to use the dashboard server, if you want to load programs regardless.