As RTDE is recommended than other ports. How can I use RTDE port in my URCaps not in daemon .Is there any resource there to develop RTDE in Java for URCaps.
Please two samples.
The latter is my developed sample.
SkyNet
Description of functionality:
Set of URCaps, libraries and examples for different purposes.
I am at very beginning of development, so for now I have an example of Dashboard server client
Hope soon I will have some more good stuff
What topics are covered:
URCap development
Requirements:
URCaps SDK v. 1.7.0
To all developer.
I have developped the urcap for monitoring I/O of Ehternet/IP.
I use the features of RTDE, XML-RPC and so on to developping this.
I want to make it better in operation.
So would you try to use this and send me your message or reply if you have the suggetions and improvements?
Regards.
GitHub
[eip1]
[eip2]
Thanks @fuikit It’s good for RTDE Input and Ouput. Is there any thing like that to moveJ in RTDE?
Thanks @fujikit In SkyNet skynet/ExampleOutputV1.java at master · o5h/skynet · GitHub
where can I get Output in that above code. Because I tried to print from startOuput and SetupOutputV1 but I didn’t got output.