UR Robot was working through Remote Mode (Ethernet IP) on our shop floor and then we shipped the robot cell down to Mexico. Powered up the line and the robot powers up fine, but Remote Mode controls are not working anymore. In the PLC Ethernet Tree, the Robot is Running and no faults or issues. I can ping the robot from cmd prompt.
- I double checked the digital inputs selections were still mapped
- verified the Ethernet Adapter is Enabled
- disabled the ethernet adapter and re-booted, then re-enable the ethernet adapter
- checked the ethernet cable to the robot controller (even ran a new one)
- Safety configuration pulls up and is enabled
- compact disk is pushed in tightly
Looking for some other suggestions…
Model: CB5 (v5.2)
UR software: 5.15.0
Build Date: 04/10/2024
Version Firmware: 41.1.79