Hello everyone! So… I have one problem with QJAR teachpendant. The problem is that when connecting the teachpendant to the computer via USB, the zimage file was deleted. Now the teachpendant only shows a black screen after restarting. I have a backup of the zimage file. Question: How can I load it back into the teachpendant if the computer no longer sees it?
Related topics
Topic | Replies | Views | Activity | |
---|---|---|---|---|
Can't Open Files from Teach Pendant | 3 | 161 | May 13, 2024 | |
Screensafer on TeachPendant while Robot is running | 1 | 341 | July 5, 2023 | |
USB port on the teach pendant vs USB port on cabinet | 1 | 1410 | September 8, 2020 | |
Could not load the program | 4 | 1249 | November 26, 2024 | |
USB file icon stuck in programs page and unable to make backups now | 5 | 168 | July 10, 2024 |