I am trying to run the trained MIRAI skill on a UR10e robot but am getting this error everytime:
Is there a way to resolve this? Is there a way to check what is causing this error?
Thank you for the help ![]()
What else is connected to the controller? Robotiq gripper?
Any other fieldbus devices?
Make sure PROFINET, Ethernet IP and MODBUS are disabled, if they are not in use.
This is the connection set-up:
these are the info about connections:
OnRobot Compute Box v3.5 (Software version 6.0.4)
F/T sensor - HEX-E/H QC
Gripper - 2FG7
Also, this is one thing I observed, when Ethernet is enabled, even simple “move” program cannot run but when I disable Ethernet it can run but cannot connect with MIRAI box.
When you say “enable/disable Ethernet”, you’re not talking about Ethernet/IP, are you? Because it’s a fairly common thing that people confuse Ethernet/IP for Ethernet TCP/IP in the UR interface.
But since you’re saying it’s working with Ethernet enabled, I guess it’s done right. ![]()
I would contact MIRAI about this issue.
thank you @efn, that gave me an idea to try. I was talking about the Fieldbus - “EtherNet/IP” in Installation menu.
New update: I got the program running by removing the OnRobot URCap, in this case it was able connect to MIRAI and find the skill and then execute it(even though the “EtherNet/IP” was disabled, it was never about about that;)). But I couldn’t operate the OnRobot gripper since there was’t URCap for that.
But, when I Re-install the OnRobot URCap, it detects the gripper but when executing the problem it shows the same error - “Protective Stop C207A0: Fieldbus input disconnected”. I am stuck now at this point.
I must admit that I’m a bit unsure if it works with two devices communicating over fieldbus simultaneously. I slightly recall having seen this issue before.
I hope someone else can elaborate on this. ![]()
Found the solution, the problem was with the RTDE registers. MIRAI and OnRobot were both using the same registers and this was the reason for this error. I updated the version of OnRobot URCap, then offset the registers and this worked.
Thank you for the ideas. @efn