Program start not working

I am currently trying to start up a machine that has 3 URs, a UR3, UR10, and UR20. The PLC is a Allen Bradley 5069 Compact GuardLogix. I have the Ethernet communications on, IP addresses set, and can send outputs from my PLC to the robots and receive inputs back from the robots.

My issue is that when I send the boolean bit to start the program the UR10 and UR20 do nothing while the UR3 actually starts the program. I will attach screenshots of the IO setup on all 3 robots. Any help on this is greatly appreciated.






Have you enabled Remote Mode in the settings menu? :slight_smile: And then using Remote Mode instead of Local/Manual?
Could be a a question of the PolyScope version maybe. The UR3e might be running an earlier version, which didn’t have the same requirements for remote starting the program.

They all have remote mode enabled when I go to start the program, my screenshots werent in remote mode when I had them on my URSIM.

I updated all of the robots when I got them to 5.16.0

Then I don’t know. The URs seem to be set up right. Are you giving the robots enough time to initialize and load the program, before you send the start command?

If the first waypoint in the program differed from the current position of the robot, you would have seen a screen prompting you to press and hold a button to align them.
Remote start methods such as IO and DashboardClient cannot automatically perform such process.

I suggest you to add
a = get_actual_tcp_pose()
movej(a, …)
at the biggining of the script(Before Start would be better)
and your next move commend must be “movej”

It would matches the current robot position to the first waypoint of the program.

This ^^

We typically put a relative move to nowhere at the beginning of all our programs for this reason.

movel(pose_trans(get_actual_tcp_pose(), p[0, 0, 0, 0, 0, 0]), a=1, v=1)

Did this solve the problem? We have the same problem running 5.17.

are you using a plc with ethernet ip? If so, you may need to update to at least 5.18 as there was a bug fix for program execution from ethernet ip.

" * In software versions 5.15.0 and above the following functions were occasionally not working when triggered through general purpose input bits: start program, stop program, initialize arm, auto start default program, auto initialize arm. This was only observed when Ethernet/IP fieldbus was enabled. Workaround for software 5.15.0 to 5.17.3 is to use dashboard server, or digital inputs. Issue is fixed in this release."

The specific issue I was having was in the Polyscope 5 revision I was using there was a major bug where the gpbi input for starting, stoping, pausing, etc. was not working at all. The have claimed to fix this by now, but since there is always a cable with extra conductors ran from our cabinet to the controller box I just set a digital input to Start and Stop the program.

Also, make sure that under Installation>General>Startup that you do not set that digital input to start the robot; do it in the IO Tab. I was told this is leftover from earlier versions and does not work. To get it to run your main program you do have to select that program in the same menu I mentioned above.