Hi, I am doing a program for a UR10 CB series, and i want to compare the position of the joints with some joint positions that i meet, but, when i run the command get_actual_joint_positions() the result that it gave me its diferent that the joint actual position if i convert the position in polyscope to rads, for example:
Now i have the follow positions at the joints:

i copy that to a variable using the command d2r like i show in the follow image:
![]()
And i use the get_actual_joint_positions()

And the result of this is:

why is diferent the result? is there a solution? and i would want to know if is there a way to convert from a Pose to a Array of Joints positions, or from an array of joint position to a Pose.
Regards