Problem with URCap content size

Hi guys,

I made a URCap installation page and it seems that the content is dense and cannot be contained
completely in just one page. This is due to screen resolution. When I tried it in the simulation, it worked because
the screen size is expandable.

Does it have any solution to this?
Can you recommend me the way to fix this issue?

Thank you in advance.
Look forward to your replied.

Please be aware, that the 12" display on the teach pendant is in fact not expandable.
The PolyScope application has a fixed dimension, and this is not alterable.
Therefore we do not recommend altering the size of the simulated PolyScope, when testing UI designs.

Either the components should be re-sized, or you should consider implementing tabs or similar sectioning of the UI.
Hence leaving less components on each page.