Increase Window of Program URSim

Your feature may already be reported!
Please search on the Feature category and sub categories, before creating one.

Summary

Increase Window of Program in UR-Sim to see all the Code

What is it?

With a Window that is capable of showing more lines in UR-Sim, complex codes can be visualized at once.
Therefore the Window that shows the Code, has to be variable in Size and Format.

Why is it needed?

Right now my code is so complex, that I have to scroll up and down a lot. A lot of mistakes happen while coding, due to the need of scrolling in the Code Window. If the Code could be visualized on a 16:9 Screen in Portrait format, the scrolling would not be neccesary anymore.

any solution so far?
I think it was possible until 5.7 or 5.8, but then … :cry: