I get Java exceptions when running it in my URsim 3.3.0.145. Could be the Java version that has caused this. Official URsim 3.3.0.145 runs 1.6.0_39
i tried to build the R3 Screwing URCap and unable to resolve the dependency of com.ur.urcap.api.ui.component.ProgramTreeNode. Please advice.
How to add a waypoint under HelloWorld sample without MoveJ
@chlai,
A Waypoint in PolyScope will always be grouped under a Move-command (MoveJ, MoveL, MoveP).
In URScript, the waypoint will be interpreted into the movel, movej or movep script code depending on which Move-command it is grouped under.
E.g this program:

Will be translated into this script code:
movej(wpt1)
movej(wpt2)
movel(wpt3)
movel(wpt4)
movej(wpt5)
I am making a command and would like to create something like the Pallet or Seek command in PolyScope Wizard. Like the StartPos under Stack.