I am studying how to use the AI Accelerator. In the UR manual there is a section to run a Demo of the Pick&Place application, and I am trying it out. After setting everything up according to the instructions, I pressed “play” to run it, but the robot suddenly lost power.
I tried to make a program with some waypoint and it ran normal. Is the cause of version 10.7? I am planning to downgrade to version 10.6 but I can’t find image of that version
Hmm… I remeber when I bought a UR5e CB5.6, the version of the control box was 10.6 (without Halt, Timer, Swith, … command). Then I update to 10.7. So I think there will be version 10.6.
Hello!
This is due to a bug in 10.7, and downgrading to 10.6 will fix it.
If you join the AI Accelerator program in centercode, you will be able to find a 10.6 image until 10.7.1 or 10.8 releases with a fix for this.
I’d recommend you report any further problems with the AI Accelerator channel on Discord which we are monitoring more closely.
See this page for links to both of the above: https://www.universal-robots.com/developer/ai-accelerator/