Hi,
I Upgraded my UR5e polyscope to new version 5.15, and running my code using latest Universal_Robots_ROS_Driver.
I’m using ROS1 Noetic version
- When dashborad’s “speed_scaling_factor” value >= 50% the ROS UR initialize crashed and I got the following message in the dashboard - “Wrist 2A: C306A3: Joint: Acceleration failed to pass sanity check”
- When dashborad’s “speed_scaling_factor” value < 50% - my Application is working fine
- Old polyscope version - my Application working fine
I downloaded the latest Universal_RobotsROS_Driver and the robot crushed when i run the following command: ```
roslaunch ur_robot_driver <robot_type>_bringup.launch robot_ip:=192.168.56.101.
its never happen with previous Polyscope versions