Photo electric sensor

Hello,

I have an Omron E3FA-DN11 2M, Photoelectric sensor. I want to feed robot with the data, Can I do that?
Or do I need some external device to connect?

Thanks

Your sensor is NPN and won’t be able to be wired to the controller directly. :slight_smile: You will need a relay between the sensor and the robot controller.
If I were you, I would get the E3FA-DP11 2M instead. It’s PNP and can be connected directly to the controller (brown to 24V, blue to 0V, black/white to DI).