Payload vs reach for UR10 CB3

I’m would like to know if I need to de-rate the payload on a UR10 CB3 when it is further from the robot mount - i.e. the robot is at its furthest reach. The documentation covers the relationship with the distance of the payload from the tool plate (i.e. wrist 3), but I have not seen anything relating to robot reach. De-rating depending on reach is common for other robot manufacturers, and feels inituitively resonable, and there was a similar question posted for the UR10e ( Payload vs Reach ), which apparently has full capacity at full reach.

Just wanted to check that this is true for the older version.

UR robots have always been specced for max payload through its whole reach.

The robots are much more sensitive to its payload and center of gravity than industrial robots due to its collaborative safety system, which is based on the current measurements of each joint.