Hi,
for a simple drawing application and cycles I would recommend the palitizer option.
an explanation is given here
to elaborate on this you could use the transpose function.
this is an example if i think more carefully, i would use a list but for a quick answer
bottom left is orgin and wp_1, up is X +, to the right is y +, in the screen is Z +
length_line = 20
ofset_1 = 10
Ofset_2 = 7
Wp_2 = transe_pose (wp_1, P [length_line * 1 + ofset_1 * 0, Ofset_2 * 0,0,0,0,0]
Wp_3 = transe_pose (wp_1, P [length_line * 1 + ofset_1 * 1, Ofset_2 * 0,0,0,0,0]
Wp_4 = transe_pose (wp_1, P [length_line * 2 + ofset_1 * 1, Ofset_2 * 0,0,0,0,0]
Wp_5 = transe_pose (wp_1, P [length_line * 0 + ofset_1 * 0, Ofset_2 * 1,0,0,0,0]
Wp_6 = transe_pose (wp_1, P [length_line * 1 + ofset_1 * 0, Ofset_2 * 1,0,0,0,0]
Wp_7 = transe_pose (wp_1, P [length_line * 1 + ofset_1 * 1, Ofset_2 * 1,0,0,0,0]
Wp_8 = transe_pose (wp_1, P [length_line * 2 + ofset_1 * 1, Ofset_2 * 1,0,0,0,0]
Wp_9 = transe_pose (wp_1, P [length_line * 0 + ofset_1 * 0, ofset_2 * 2,0,0,0,0]
Wp_10 = transe_pose (wp_1, P [length_line * 1 + ofset_1 * 0, Ofset_2 * 2,0,0,0,0]
Wp_11 = transe_pose (wp_1, P [length_line * 1 + ofset_1 * 1, Ofset_2 * 2,0,0,0,0]
Wp_12 = transe_pose (wp_1, P [length_line * 2 + ofset_1 * 1, Ofset_2 * 2,0,0,0,0]
Wp_13 = transe_pose (wp_1, P [length_line * 0 + ofset_1 * 0, ofset_2 * 3,0,0,0,0]
Wp_14 = transe_pose (wp_1, P [length_line * 1 + ofset_1 * 0, Ofset_2 * 3,0,0,0,0]
Wp_15 = transe_pose (wp_1, P [length_line * 1 + ofset_1 * 1, Ofset_2 * 3,0,0,0,0]
Wp_16 = transe_pose (wp_1, P [length_line * 2 + ofset_1 * 1, Ofset_2 * 3,0,0,0,0]
I hope you understood this and also understand how to do the oblique lines. and for offset Wp_x_offset = transe_pose (wp_x, P [0,0, -0.02,0,0,0]
but I would recommend using palitizer then with each item:
Wp_1 = get current tcp_pose ()
Wp_2 = transe_pose (wp_1, P [length_line, 0,0,0,0,0]
move L (wp_1_offset)
move L (wp_1)
move L (wp_1)
move L (wp_2_offset)
(for a script move you also need to add ad speed and acceleration, but don’t know this by heart, look it up in the script manual.the script I wrote I did quickly, so some errors may occur)
maybe someone will come up with a better idea, but I hope to point you in the right direction.
Regards,
Corné