Hi,
Here’s a complement for my previous topic
First :
roslaunch ur_robot_driver ur3_bringup.launch robot_ip:=10.31.56.102
When I use MoveIt! :
roslaunch ur3_moveit_config ur3_moveit_planning_execution.launch
rostopic echo -n 1 /tf
transforms:
-
header:
seq: 0
stamp:
secs: 1632812531
nsecs: 683076397
frame_id: "base"
child_frame_id: "tool0_controller"
transform:
translation:
x: 0.40397276508452934
y: -0.05284395305852813
z: 0.2684066473605699
rotation:
x: -0.8404507390466658
y: 0.5410578077432447
z: 0.029860070618397676
w: 0.0027166336984866496
---
Here, X is positive and Y is negative. It corresponds to the real robot and to the TCP coordinates displayed by the teach pendant (X = 403.98 mm and Y = -52.83 mm). So, OK.
Now, if I use this code :
import sys
import rospy
import moveit_commander
moveit_commander.roscpp_initialize(sys.argv)
rospy.init_node('move_group_python_interface_tutorial',anonymous=True)
robot = moveit_commander.RobotCommander()
group = moveit_commander.MoveGroupCommander("manipulator")
print(group.get_current_pose())
I get this :
header:
seq: 0
stamp:
secs: 1632813992
nsecs: 777175188
frame_id: "base_link"
pose:
position:
x: -0.4033402964629966
y: 0.05497579606279141
z: 0.26930932855449635
orientation:
x: 0.5431377755932296
y: 0.8391674130280562
z: -0.0012092217977459708
w: 0.028247963078459875
Now, X is negative and Y is positive, but Z is the same than previously. Not OK!
We can notice too that orientations are not the same but the robot was in the same position/orientation (I don’t move it between the two experiments)
Why and how can I correct this to have good values with get_current_pose()?
Thanks,
Philippe