Hi,
I run this :
roslaunch ur_robot_driver ur3_bringup.launch robot_ip:=10.31.56.102 kinematics_config:=${HOME}/Calibration/ur3_calibration.yaml
then this :
roslaunch ur3_moveit_config ur3_moveit_planning_execution.launch
Now, when I run this commands :
import sys
import rospy
import moveit_commander
moveit_commander.roscpp_initialize(sys.argv)
rospy.init_node('move_group_python_interface_tutorial',anonymous=True)
robot = moveit_commander.RobotCommander()
group = moveit_commander.MoveGroupCommander("manipulator")
print(robot.get_current_state())
print('============================')
print(group.get_current_pose())
It prints this :
[ INFO] [1632386727.339775158]: Ready to take commands for planning group manipulator.
joint_state:
header:
seq: 0
stamp:
secs: 0
nsecs: 0
frame_id: "base_link"
name:
- shoulder_pan_joint
- shoulder_lift_joint
- elbow_joint
- wrist_1_joint
- wrist_2_joint
- wrist_3_joint
position: [-0.12209493318666631, -1.7235949675189417, -0.9860222975360315, -2.003582779561178, 1.5696308612823486, 1.4477026462554932]
velocity: []
effort: []
multi_dof_joint_state:
header:
seq: 0
stamp:
secs: 0
nsecs: 0
frame_id: "base_link"
joint_names: []
transforms: []
twist: []
wrench: []
attached_collision_objects: []
is_diff: False
============================
header:
seq: 0
stamp:
secs: 1632386727
nsecs: 548035383
frame_id: "base_link"
pose:
position:
x: -0.2999829298506016
y: 0.15009632025728392
z: 0.4000202051437085
orientation:
x: -0.9999996330797376
y: -0.0004935850271520933
z: -0.0004722812120140486
w: 0.0005168797421440206
On the UR3 teachpad, I can read that, for the base feature, the TCP coordinates are :
X = 301.2 mm
Y = -148.3 mm
Z = 399.4 mm
RX = 0.012 rad
RY = -3.14 rad
RZ = -0.003 rad
We can see that the Z coordinates are the about same (teachpad => 399.4 mm and python => z: 0.400) but the X and Y coordinates are opposite sign (teachpad => X = 301.2 mm but python => x: - 0.299)
Why? How can I correct this?
Best regards,
Philippe
base
and base_link
are not the same, but are rotated by 180 deg.