Hello everyone, I’m a student that currently working on a pick and place project based computer vision as the input data. For the hardwares, in this project I’m using:
- a Logitech webcam camera planted on a UR5e wrist
- PC and Ethernet cable
- UR5e with RG2 gripper
And also:
- Ubuntu 18.04
- ROS Melodic
- Universal_Robots_ROS_Driver.
I have changed the action ns in ros_controllers.yaml to scaled_pos_joint_traj_controller/follow_joint_trajectory .
And I tested on the terminal :
roslaunch ur_calibration calibration_correction.launch \robot_ip:=192.168.0.100 target_filename:="${HOME}/my_robot_calibration.yaml
roslaunch ur_robot_driver ur5e_bringup.launch robot_ip:=192.168.0.100 [reverse_port:=REVERSE_PORT] kinematics_config:=/home/tazkia/my_robot_calibration.yaml
roslaunch ur5e_moveit_config ur5e_moveit_planning_execution.launch limited:=true
roslaunch ur5e_moveit_config moveit_rviz.launch rviz_config:=$(rospack find ur5e_moveit_config)/launch/moveit.rviz
And then drag the ball in front of UR in Rviz, click Plan, and then click Execute, and the robot moves. So the driver works for me and I have no problem. 
The opencv python program is also ready. The output data is X and Y coordinates (because the Z or depth will be made as an absolute value) and the rotational angle value in Yaw axis which later to control wrist 3 / end effector of UR.
For the python script, many people try to use test_move.py from the previous driver but Universal_Robots_ROS_Driver doesn’t come with that. So which python script program that can be sent to control the robot?
But I still don’t understand how to process this data (x, y, and theta) of the object in a frame and turn into global coordinates of UR5e, and then should I use inverse kinematics inside the code program or just simply send as the end effector pose goal to the robot? And then after I combine the python script of image processing and python script to control the robot, the final is how to send / call this one python script file to make the robot moves?
Thank you everyone, I really need your help to graduate from this undergrad :”) Have a good day ^^