Multiple robot ethernet connections to AB PLC

Hello - I have 3 robots networked ethernet together on AB PLC (Compactlogix) for some reason, only one will connect, the other two always show faulted. Is there different settings (other than IP address) that must be applied in the Generic ethernet module if more than one UR is connected?