There’s not an “easy” way, as in there’s no checkbox to say “Mirror Pose” but you can create Line Features and teach all points relative to that Feature. It’s possible to then just multiply a certain axis’s value by -1 to “mirror” it around that Feature. The hard part can be to make the orientation also mirrored. If it was pitched at 45 degrees, now it needs to pitch -45 degrees. Defining that behavior can be tricky. But it should be possible with pose manipulation and Features.
Well, the most important thing for me is to mirror the pose, because other whise i just would use the other local coordinate system. But as it is a 3D gluing programm with a lot of turning the TCP without cutting the hoses, i only can mirror the program or write it new.
I just get the feeling with your suggestion, that making new programm would be easier in the end…