Loading installation file

Hello,

I have been using a UR10 for loading CNC lathes for a year now.

I want to make a template program for the UR10. so that I only have to enter some variables for the different article that we make on the CNC lathes.

variables that I include in my program are:

  • product width
  • product length
  • product height
  • product weight

I want to save these programs per article so that when the same article is requested again, I can load the program and start it without having to set it up again.

I would like to use the same installation file for each of these programs. but I notice that when I open/import existing programs it automatically opens the corresponding installation file. with which it was previously made. while I would like it to point to the same installation file at all times.

can anyone help me with this issue?

Kind regards,

Dennis Verberkt