How to use the third-part .jar files?

I got it to work. In order to add and use the package I did that:

  1. Add the package to dependencies:
    <dependency>
    <groupId>com.sun.jersey</groupId>
    <artifactId>jersey-client</artifactId>
    <version>1.8</version>
    </dependency>

  2. Add the package with an preceded exclamation mark to Import-Package:
    <Import-Package> com.ur.urcap.api*;version="[1.1.0,2.0.0)", !com.sun.jersey.api.*, *</Import-Package>

  3. Add the ArtifactId to Embed-Dependency:
    <Embed-Dependency>jersey-client</Embed-Dependency>

I did not manually add any jars to my resource folder or so. After a successful building I got an error while starting polyscope, that an additional package com.sun.jersey.core is missing. Apparently the jersey-client package has additional dependencies which need to be included as well. So I had to add jersey-core and javax.mail to dependencies and also to Embed-Dependency and then it worked. The required jar files got added automatically to the urcap file.

I hope this helps a bit :wink: