My question is about how the setup/update of the installation variables (Installation > General > variables) via URCap works.
I will setup/update the value of the variables into an Installation Node by presenting a simple interface to the user. After the setup/update phase the user can access the value into the Program page.
I don’t even sure if this is possible, thanks for help.