Hi, is there an easy way to mount a VMWare share in URSim?
I’ve tried this command without success:
sudo mount -t vmhgfs .host:/ /mnt/hgfs/
or
sudo mount -t vmhgfs .host:/ /home/ur/shares/
I’m getting the error: “Error: cannot mount filesystem: No such device”.
If I type the command “vmware-hgfsclient” in terminal I get the VMWare share listed up.
Hi Daniel,
I am not that familiar with VMWare, I use Oracle VM VirutalBox instead but here is a quick google search results I came up with → VMware Workstation Pro Documentation
It sounds like you didn’t setup the networking setting portion of the setup.
Thank you for the feedback. I tried to mount a windows share, but I got the error message “mount: unknown filesystem type: smbfs”.
I was wondering how to access the shared folders set up in the settings of the virtual machine in VMware workstation.
It should be possible since the mount command in URSim/lubuntu does support vmhgfs.
Create somewhere on your PC a folder called “VM_Shared”.
Go on the settings of the VM than you created. Go to “Shared Folders” and add the folder than you created. “Auto-mount” and “Make Permanent” have to be selected.
Play the VM.
Open a terminal (CTRL+ALT+T) and write:
Sudo adduser ur vboxsf
Reboot.
The shared Folder will be inside of : /media
This method is working for me 
Thank you for the tip which I’m looking for. I believe it will wok in Virtual Box, but not in VMware.
Maybe I’ll switch to Virtual box to test it out.