Dear UR+ Development Support
We are developing new view at UR Caps to define signal names. See follow image “View1”
For example “digital_in[2]” —> digital_in[2]: Start program
As result we want set new name “Start program” into I/O Setup and display it. See follow image” View2”
Please tell us which function should be used? We cannot find in “scriptManual.pdf”.
Also it should change default.installation or not?
Thanks
TFSOFT
thph
July 22, 2019, 12:47pm
2
Using the API of the IO, the following methods can be called → link:
https://plus.universal-robots.com/apidoc/53887/com/ur/urcap/api/domain/io/io.html
Which means that we can only retrieve information about the name of the IO, but the api does not support setting name of the IOs. This could be a feature request.
thph
Thank you very much!
We will use the I/O Setup to set signal names.
And hope your new version coming soon.
Thanks again.
TFSOFT