GCode post processor from Fusion

I’m trying to post from Fusion 360 using the built in Universal Robots post processor. NC Extension is .txt which seems odd but when I post, it creates a .txt file that says “This is a dummy file.Your program files are located here: C:\Users\jbenn\Desktop\1001”. Then the 1001 folder is just an empty folder.

Any thoughts?

Hi, I’m facing the same issue. Any news would be welcome.
Thank you.

Coming back to this, I’ve solved it just by unticking the box “Use subfolder”.

2 Likes

I also facing the same issue but I confused it . Please explain more clearly about this.

has anyone found any solutions to this issue. I tried the suggestion above but no dice.