Feature Request: URScript Matrix Element Indexing Improvement

URScript Example:

a = [[1, 2], [3, 4]]

b = a[0,0]

c = a[0]

the result of b is 1 as expected

the expected result of c is the first vector in a, [1,2], but instead is:

'Index out of range'

Could we access a multidimensional element using one of the following?

c = a[0,]
c = a[0]

What were the results you expected to receive for b and c?

Thanks Matt, just updated the first post. Looking to get the first vector ([1,2]) like you would get the first pose in a list of poses.

What is the language you used for this example? It looks like it is python

The issue I see is with array b not c. to get a specific value in python, you have to declare as b=a[0][0], not as a[0,0].

The array c might be initialized to a size 1 or 0. I would check for an issue on your code because the ‘Index out of range’ is an error message from the python side.

check this example:

Ooh appreciate your response but this in URScript. Believe me I would also like slicing and negative indexing like in python but I’ll settle for the basic features for now haha.

Give it a try using the new matrix/multidimensional array functionality in SW 5.9 and see what you get.

Derp, I completely skipped over the part where you said URScript on the first post. My bad, :smile:.

Hi, I have the same problem of indexing one column/row of a matrix. Did you solve it?

def get_element(mat, i, j):
     temp = mat[i]
     return temp[j]
end

Thus solving the problem forever, issue closed /s

opposite for assignment

Edit: This was wrong, update here:

HI Terry, thank u for the support. I’ve tried to add this script in polyscope, but it failed the execution.
I’ve an error with temp = mat[i] with the following message: the variable Matrix is not indexable!

Ooh, yea you’re going to hate this more but what we actually did is used the tried and tested @mbush technique and used another language to generate this:

def get_element(mat, index, size):
    if size == 1:
        temp = 0
    elif size == 2:
        temp = [0, 0]
    end  # continue this trend
    count  = 0
    while count < size:
        temp[size] = mat[index, size]
        count = count + 1
    end
end

matrix = [[0, 1], [2,3]]
element_size = 2

# Output is [2, 3]
row = get_element(matrix, 1, element_size)

That’s insane. There is no way to index a row/column in 2022. UR must do more on the programming side.
Thank u @terryc for the support!

No problem! My favourite URScript feature is using other scripting languages to procedurally generate missing functionality.

Hello, actually even try your on urscript for an UR20. The code is actually a little bit different:

def get_element(mat, index, size):
    if size == 1:
        temp = 0
    elif size == 2:
        temp = [0, 0]
    else:
        temp = [0] * size  # General case for larger sizes
    end
    count = 0
    while count < size:
        temp[count] = mat[index][count]  # Access elements correctly
        count = count + 1
    end
    return temp
end

It works for me hope it can help someone else.