Hello,
We have an UR3e. I’m very new with EtherNet/IP and trying to get/set the digital input/output of our UR3e with EtherNet/IP. Our final goal is to use the open-source library to communicate with UR3e using EtherNet/IP Implicit Messaging.
Our first target is EEIP library. In the proposed example, it can get/set with the PLC Wago based on the CIP Classes defined in Wago datasheet (Table 153 and 155, page 190). However, when I check the eip-iomessage file proposed officially by Universal Robots in here, the physical address space are organized differently (not by CIP Classes).
Could anyone give me some advice so I can achieve the goal? Thank you.