Connecting Cobot to Siemens Logo!

Hi, is it possible to connect a Siemens Logo! to a UR5e or a CB3 via ethernet?

Hi @chrispocock,

I“m not really sure if a LOGO can have a signal exchange with the UR.

I“ve implemented a comminucation between a S7 1212 and the UR (10e).
And to make them both ā€œtalkā€ to each other, u have to open a communication (connection) via a Siemens
FB (TCON).
I don“t think you can do that with a LOGO (but tbh I“m not very familiar with LOGO).

For what do u need the connection between the UR and the Logo?
What you wanna do/see?

Greetings from Luxembourg!

Hey,

You should be able to use Modbus TCP and communicate between the registers of the UR and Logo. I am going to try it myself shortly and get back on this.

BR

please find my example here with a complete documentation. this one will hopefully explain everthing.