Hi,
when i create a Waypoint with the URCap Api it adds the Waypoint under a MoveNode and its Configuration is shown like this:
when i click “Set Waypoint” all seems normal and the below Menu is openend:
Note that the Robot Position is the same as shown in the Animation in the Waypoint Menu.
The Problem is when i click “Edit pose” it does not calculate the TCP Offset and the Robot is using its tool Flange as TCP:
it seems that this is a Representation Problem. When i Cancel the “Edit Pose” Menu everthing is fine.
This only occurs when creating the Waypoints through the URCap API.
inu
July 12, 2018, 8:41am
2
How did you generate the waypoint?
i’m adding it through the URCap API Version 1.3.55
This Problem also occurs in the Ellipse example Program
My TCP Config is:
X: -0.77 mm
Y: -21.25 mm
Z: 415.2 mm
RX: 1.9246 rad
RY: -1.8169 rad
RZ: 0.5600 rad
Hi, since I have a similar problem, is there any solution available ?
Or, when can we expect a solution ? We need it really for our customers who do like to start using our URCAP.
Thanks.
Our temporary solution is telling our customers do not use edit Pose.
Ohh. Temporary = 4 months already ??
Yes, this seems to be the only work around, but this is not a solution I think. …
Another workaround is to program custom waypoint urcap nodes which we did already…
Problem also occurs in the new e-Series
@jbm please fix it
jbm
November 14, 2018, 9:18am
8
Which version of PolyScope and URCap API is used?
PolyScope 3.6.0
with api 1.2.56
Samen happens with 3.7.0; please check also problem with getuserdefined robot position .
jbm
November 14, 2018, 11:42am
11
We are investigating the issue.
jbm
December 6, 2018, 10:06am
13
Error has been reproduced, and a fix is planned for next minor release (3.9/5.3).
This Problem:
Hi,
i faced another Bug when creating API generated Waypoints with a TCP Offset of
Z = 400 mm:
when i create a Waypoint with this Pose through the Polyscope UI:
[grafik]
everything is fine:
[grafik]
but if i use the same Pose for a API generated Waypoint i get an Error that the Inverse kinematics could not find a solution:
(Ellipse Example)
[grafik]
[grafik]
Please note that this has nothing to do with reachable Ellipse Points it is just an example to reproduce the error. It even c…
still occurs on PolyScope Release 5.3 using API 1.5.0
Did i miss something that must be changed through the new API 1.6.0 ?
jbm
March 22, 2019, 10:08am
16
Can you verify, that the problem listed in this topic is resolved in 3.9/5.3?
The behavior wrt. the Ellipse example is unrelated.
jbm
March 25, 2019, 11:57am
17
This issue is resolved in PolyScope 3.9.
Release of URCap API 1.6.0, PolyScope 5.3 and PolyScope 3.9
Dear valued developers,
Universal Robots is delighted to announce, that we are now releasing a new software, to continuously deliver more value to you and our customers.
The new release consist of:
PolyScope 5.3.0 for e-Series
PolyScope 3.9.0 for CB3
URCap SDK 1.6.1 including URCap API 1.6.0 for both platforms
Key features
The key features in this release is:
API
Support for configuring TCP’s on Move nodes
Parent nodes can now s…