Our production have sometimes the problem to push the “Play” Button on the Monitor. Maybe it is possible to make it bigger.
This is noted, however also note, that it is possible to mount an external PLAY button to a digital input, by configuring it so in the IO Setup screen.
We’d like to see bigger buttons on the run screen as well, or allow us to configure the pendant layout for run mode only.
We already have external buttons solely for this purpose but would love to not have to add this nor use up 3 inputs to make operator friendly buttons.