Hello,
I´ve got the task to create a URCap where the programm has to be altered / created from an external source.
So my jurney get me to write a Installation Node which is connecting to the external source via sockets.
The Installation Node should afterwards be able to receive commands and create/alter Nodes in the Programmtree.
Is there a way to access the Programmtree from the installation node?`
I found URCapAPIFacade.getURCapAPI().getProgramModel();
But getURCapAPI() is marked as deprecated. And via the suggested getSystemAPI(), the needed elements seems not to be reachable.
Thanks in advance!
I thought about different approach then yours, but maybe it will be helpful for you:
- Add to your “Robot program” tree “Script” element (Left menu -> Advanced -> Script) and change “Line” to “File”. Choose file name and save it. This file is located in “programs” directory on UR.
- Then you can externally change content of this file (for example you can connect with UR via sshfs on Linux).