Hi All,
So my (newest) problem is we are palletizing boxes off of a conveyor belt onto a double pallet system and when being placed need to have the label facing out.
The program we use currently is terribly buggy and doesn’t use the palletizing wizard to do this (presumably because of the two pallets). I am in the process of trying to write a new code to palletize using the wizard since it seems to be a much easier option.
I am using the square pattern currently with a pose save and add product height since I need to add a slip sheet every 2 layers on the pallet and this was the easiest way I could find to accomplish this. However, with the pallet wizard since you only set the initial point is there a way to add rotation to half of the boxes on the pallet?
I apologize for the many questions I am just trying to learn about these robots as I go. Thank you in advance!