Hey everyone,
I need your help for creating children node when I push a button.
I want a structure like that:
Inside of the program node I want to have a button for creating a child node (this child will be used for select differents parameters and sending the parameters to a machine).
Inside of this child I want another child called with another button ( this child is a moveL but I wont add a normal moveL because I will change the speed with the parameters by example).
URCapname
–Child (1)
----SpecialWaypoint
----SpecialWaypoint
–Child (2)
----SpecialWaypoint
----SpecialWaypoint
Hi Anrnaud,
you could take a look at the pickorplace
-sample URCap.
There it is shown how you can add your own custom nodes via the pressing of a button.
For the configuration and insertion of usual programnodes like movel
the ellipse
-sample serves as a good template.
ok thank you for your reply it was really helpful
And is it possible to hide the move P inside of my childNode I mean than I’ve add my child node and after that I will just need to add the waypoints or the circle move.
If you want to use the waypoints provided in Polyscope, I see no way around it.
But you can create your own custom waypoints in the URCap as programnodes and add the functionality you need. Add a button and read out the current pose for example. Then you can store it a movep
-command in the Script-Writer.