Hello everyone,
I’m currently working with a UR5e.
I’m developping some URCaps using the virtual machine 5.9.4.1031232
I need to activate some outputs from a g-code file.
I have seen that this is possible to do :
(source : Universal Robots - Remote TCP & Toolpath URCap FAQ)
But the robot on the virtual machine is on version 5.11.0 and not 5.11.5.
Do I have to update the virtual robot or there is another way to activate some outputs ?
If an update is needed, how can I update the virtual robot ?
(The outputs need to be activated at some specific positions given by the g-code file. I cannot activate thme separetly by a Set fonction or from an URScript)
Thanks in advance for your answer
Best regards