Wire for connecting Digital I/O

Hello everyone!

I made a programm for a robot and now I need to connect the Robot I/O the following interface

I’m not used to electrical components and need to get the wires to connect the robot I/O and this.
I was thinking about getting something similar to this and wanted some advice

0035832 Lapp Kabel, Câble multipaire non blindé, Données, Par M | Farnell FR

Thanks,

There’s no need to use 1mm2 wires (if you’re not using an external PSU for 24V > 2A). :slight_smile: 0.5mm2 will do just fine.

Aside from that, you should take into account whether the cable will be stationary or move around a lot. PVC cables are good for stationary applications, whereas PUR cables are more flexible and durable to being flexed often (mounted on the robot for example).